{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is an SCF1 fault on the ATV12 drives?
Issue:
SCF1 on ATV12 drives.

Product Line:
ATV12

Environment:
All

Cause:
Getting an SCF1 fault on the drive.

Resolution:
This is a Short-circuit fault or grounding fault at the drives output.

Suggested things to check :
-Disconnect the motor and Megger out the motor with 1000v Megger.
-Check all the cables connecting the drive and motor.
-Try running the drive with the motor disconnected to do so set OPL (FLt menu) to no and run the drive at 15, 30, 45 and 60 Hz and measure the output voltages with a digital RMS meter to see if all of the voltages are balanced.
-Replace the drive if needed.
-Replace the motor if needed.

Schneider Electric Global