Issue:
ATV212 conformal coating
Product Line:
ATV212
Environment:
All
Cause:
N/A
Resolution:
ATV212 is Conformal coated per IEC 60721-3-3 classes 3C1 and 3S2 (chemical gases & solid particles).
ATV212 conformal coating
Product Line:
ATV212
Environment:
All
Cause:
N/A
Resolution:
ATV212 is Conformal coated per IEC 60721-3-3 classes 3C1 and 3S2 (chemical gases & solid particles).
Released for:Schneider Electric Global
Issue:
ATV212 conformal coating
Product Line:
ATV212
Environment:
All
Cause:
N/A
Resolution:
ATV212 is Conformal coated per IEC 60721-3-3 classes 3C1 and 3S2 (chemical gases & solid particles).
ATV212 conformal coating
Product Line:
ATV212
Environment:
All
Cause:
N/A
Resolution:
ATV212 is Conformal coated per IEC 60721-3-3 classes 3C1 and 3S2 (chemical gases & solid particles).
Released for:Schneider Electric Global