{}

Welcome to the Schneider Electric corporate Website

Search FAQs
What programming software is required to support the TSX07 Nano PLC?

Article available in these languages: Japanese

Issue
Need to identify the programming software for the TSX07 Nano PLC.

Product line
PL7-07, TSX Nano

Environment
TLXLPL707P40M

Resolution
PL7-07 is required to support the TSX 07 Nano PLC. The part number for a single install is TLXLPL707P40M. Note that this is an obsolete DOS based software. There is no windows based equivalent software.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: