Search FAQs
What is the part number for the USB cable to connect a Modicon M340 to an Magelis XBTGT2000+ series, Harmony HMIGTO, HMIG3U series?
Issue
What is the part number for the USB cable to connect a Modicon M340 to an Magelis XBTGT2000+ series, Harmony HMIGTO, HMIG2U, HMIG3U, HMIST6 series?
Product Line
Modicon M340 PLC
Magelis XBTGT
Harmony HMIGTO, HMIG2U, HMIG3U
Harmony HMIST6
Environment
HMI to PLC Modbus Communication
Resolution
Schneider Electric offers 2 different length of USB communication cables to connect a Modicon M340 to one of the above HMI families using the Modbus TCP-USB protocol:
USB Cable Part Number | Length |
BMXXCAUSBH018 | 1.8 meter |
BMXXCAUSBH04 | 4.5 meter |
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: