{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

What is the accuracy of the RM17TU00 adjustment under voltage setting?

Goals and Symptoms

If I set the voltage to 208V nominal, then I set the under voltage trip point at -5%, that's = 198V. What it the accuracy of the 198V under voltage setting? Does the relay trip anywhere in between 178V-218V?? (+-10% of 198V ???)

Facts and Changes

accuracy of dropout when set for a particular percentage.
RM17TU00

Causes and Fixes

The accuracy of a voltage setting is given in catalogue by the "setting accuracy" characteristic. It is the accuracy of the potentiometer position according to the marking on the front face.
Example:
Set the potentiometer at -10% (with Un= 208V => 187V), then the real voltage setting will be between 9% and 11% of Un(185V and 189V), +/-10% of 10.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: