undefined undefined
{}

Welcome to the Schneider Electric corporate Website

Search FAQs
Maximum torque for the connections of the time relays RE11. Maximum length that you could peel the cable ?

Goals and Symptoms

Maximum torque for the connections of the time relays RE11.
Maximum length that you could peel the cable ?

Causes and Fixes

The maximum torque for the connections of the time relays RE11 is 1Nm, screew M3 / CEI 947-1
The maximum cable peeling length for connexion is 8mm.


Legacy KB System (APS) Data: RESL192132 V1.0, Originally authored by LaBe on 06/16/2008, Last Edited by LaBe on 06/16/2008
Related ranges: Zelio Time

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
move-arrow-top