{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
IONE6.0: Error in setup log: "Creating maintenance jobs: PMLMSDEManager: ActiveX component can't create object"


ION Enterprise user may notice that SQL Jobs (such as Maintenance, Backup. Archive & Trim etc. are missing from the ION Enterprise system.

Inspection of the "ION Enterprise6.0Setup.log" file may show the following error:
---------------------------------------------------
OK (0) 6/17/2011 1:55:46 PM Error (-2146827859) Creating maintenance jobs: PMLMSDEManager: ActiveX component can't create object
---------------------------------------------------
This error is associated with 64-bit operating systems trying to execute the VB script that is normally called by the IONE installer using the 64-bit version of wscript.exe. The resolution to this issue can be found near in

RESL203761

Legacy KB System (APS) Data: RESL209556 V1.0, Originally authored by DaMi on 11/02/2012, Last Edited by DaMi on 11/02/2012
Related ranges: ION Enterprise V6.0

Schneider Electric Global