{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to Add / Modify Modems for ION Enterprise

Issue
Customer has a modem type that is not in the ION enterprise modem database and would like to add a new modem.

Product Line
ION Enterprise

Environment
ION enterprise modem database

Cause
If a customer has a modem type that is not in the ION Enterprise modem database, it is possible to add a new modem

Resolution
To configure custom modem settings:

  1. Download the nonmodem setup tool from the FTP site
  2. Visit the modem manufacturer web site to get the AT strings.
  3. You will need to copy a modem setting (so that USER appears after the modem type) then you can adjust the settings & save. This will then be available in the management console as a selectable modem type.
    config

Schneider Electric Global

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: