{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can Total Demand Distortion (TDD) be manually calculated?

Total Demand Distortion (TDD) can be calculated by the following two methods.
*Note you will need the Peak Demand Current.

1) If the per phase THD and Fundamental currents are known, the attached calculation can be used.

Image 1


2) If the per phase thd and true RMS currents are known, the attached calculation can be used.
Image 2

Schneider Electric Global