{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
PM600 Series Available Onboard Alarms

Issue
What onboard Alarms are available for PM600 Series meters?

Product Line
PM600
PM620
PM650

Environment
Onboard Alarming Capability

Resolution
There are no onboard alarms available for the PM600 and PM620 meters, however, PC Based alarming can be created via software.

The PM650 does have onboard alarming capabilities (30 alarm conditions). See page 66 of the PM600 Series User Guide

Schneider Electric Global

Attachment(s)
PM600_Series_Instruction_Bulletin.pdf [1.39 MB]