{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Will the EGX models communicate with the older CM100 and CM200 lines?

Issue:
Will the EGX models communicate with the older CM100 and CM200 lines?

Product Line:
CM100 and CM200 series
EGX100
EGX200
EGX300
EGX400

Environment:
Communication capability between EGX gateway and CM100/CM200 series meters

Resolution:
Yes, EGX models (EGX 100, 200, 300, and 400) will communicate with the older CM100 and CM200 meters.

NOTE: Customer will have to configure the "Device List" from EGX webpage. Configure the modbus address and set protocole as "PowerLogic". View picture below where '1' is the CM100/200's modbus address:

Schneider Electric Global