Search FAQs
How can I share a single CT and PT for two or more Meters?
Issue
The User would like to use a PT (potential transformer) or a CT (current transformer) for two separate meters..
Product Line
PowerLogic and ION Meters
Environment
Current Transformers and Potential Transformers
Cause
Typically each power meter has its own set of CT's and PT's. It may be desirable to share a voltage or current source from one of the PT's or CT's.
Resolution
The ION and PM meters can share CTs and PTs with other meters.
Take PM1200 and three phase 4 wire connection for example, the wiring should be like below:
Also,this wiring can be used in other PM and ION meters.
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: