{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

What is IONTest, and how do I use it to read meter data?

Product Line
ION Enterprise
Struxureware Power Monitoring (SPM)
Power Monitoring Expert (PME)

Resolution
IONTest is a program that allows for very specific communications to ION devices. It removes the Graphical User Interface from the communication path in favor of a more direct connection to the ION Device.  This allows for in-depth troubleshooting, such as setting modules online/offline, changing module parameters, deleting modules, and requesting information. This information can then direct an issue to the meter side or the software side for a solution.

There are three areas in an IONTest message: a handle, a method, and a value.

The handle describes what object you are performing your action on.
The method is what action you are taking on the object referenced by its handle.
The value is the value(s) provided to the method to perform its operation.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: