{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

Logipam (SFT2885) Manual for Sepam Series 80

Issue:
This document can be useful to understand how to use and test the Logipam Software (SFT2885) for Sepam Series 80 Relays.

Product Line:
Sepam Series 80 Relays

Environment

Cause

This article provides some basic information about the the Logipam software (SFT2885) and where to find the manual in the KB. The full name of this Logipam Manual is:
----------------------------------------
Logipam
SFT2885 Programming
Software
for Sepam series 80
Users Manual
SEPED303004 eng Version 2
-------------------------------------

Resolution

  • Logipam (SFT2885 software) is used to program control system functions for Sepam series 80.
  • Logipam runs in MS Windows.

Programming Language

  • The programs are created in Ladder language.
  • Ladder language is a graphic language used to transcribe ladder diagrams. It uses the basic graphic symbols of a diagram: contacts, coils and connections.

When Should Logipam Be Used?

  • Logipam is used to create specific functions or to complement Sepam predefined functions.
Composition of the Logipam Software
  • Logipam consists of:
.. A program editor in Ladder language

.. A simulator for checking that the program is working correctly

.. A code generator for executing the Sepam program



Schneider Electric Global

Attachment(s)

Logipam SFT2885 - User’s Manual_SEPED303004EN_01-2013.pdfLogipam SFT2885 - User’s Manual_SEPED303004EN_01-2013.pdf [1.11 MB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: