{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

Video: ION Enterprise/SPM/PME - How to Create/Register a custom ION Virtual Processor Service (VIP)

Issue
Some systems with extensive computer based programming to aggregate separate meter data will require multiple VIP nodes for proper operation.
This document outlines how to create these additional VIP nodes.

Product Line
ION Enterprise
Struxureware Power Monitoring
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Environment
All ION Enterprise and Power Monitoring Expert systems.

Cause
For proper performance each VIP should contain both a .cfg and .bak file.  These files should max at approximately 2 Mb.  Once this file size is reached, for the integrity of the system, it is recommended to create a new VIP for further PC based programming.

Resolution
Create a new ION Virtual Processor Service (VIP) and start it using the following steps:

  1. Open a command prompt window by right-clicking on CMD and selecting "Run as administrator."
  2. Using cd navigate to ...\Power Monitoring Expert \System\bin *
    1. Example: If PME has been installed on the C drive type cd C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\system\bin
  3. Register the Virtual Processor as a service by typing "vip.exe -Service -N<custom VIP name>"
    1. Example: For a VIP named PMEServer type vip.exe -Service -NVIP.PMEServer or vip.exe -Service -NPMEServer
  4. Close the command prompt window.
  5. Open Control Panel > Administrative Tools > Services and start the newly registered VIP


*Note:
The path for older versions or direct in place upgrades could be as follows
...ION Enterprise\System\Bin

Video: ION Enterprise/SPM/PME - How to Create/Register a custom ION Virtual Processor Service (VIP)



Refer to the below image for information on registering related services:Video: ION Enterprise/SPM/PME - How to Create/Register a custom ION Virtual Processor Service (VIP)

Schneider Electric Global

Explore more
Range:
EcoStruxure™ Power Monitoring Expert Building EditionEcoStruxure™ Power Monitoring Expert 8.2EcoStruxure Power Monitoring Expert
Explore more
Range:
EcoStruxure™ Power Monitoring Expert Building EditionEcoStruxure™ Power Monitoring Expert 8.2EcoStruxure Power Monitoring Expert
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.