Search FAQs
What are the default format link parameters for Modbus communication with SoMove?
Issue:
Modbus format parameters
Product Line:
ATS48, ATV32, ATS22, ATV12, ATV212, ATV61, ATV71, ATV31, ATV312
Environment:
All models and serial numbers
Cause:
None
Resolution:
Parity = Even, Stop Bits = 1, Baud rate = 19200. Please note: The ATS48 has no parity as the default value. You must either change the format in the ATS48 to 8E1 or change the parity in SoMove to 8n1.
Modbus format parameters
Product Line:
ATS48, ATV32, ATS22, ATV12, ATV212, ATV61, ATV71, ATV31, ATV312
Environment:
All models and serial numbers
Cause:
None
Resolution:
Parity = Even, Stop Bits = 1, Baud rate = 19200. Please note: The ATS48 has no parity as the default value. You must either change the format in the ATS48 to 8E1 or change the parity in SoMove to 8n1.
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: