Search FAQs
What can cause a CFI fault?
Issue:
Display shows CFI
Product Line:
ATV71, ATV71
Environment:
All models and serial numbers
Cause:
Invalid configuration. The configuration loaded in the drive via the bus or communication network is inconsistent.
Other cause is Max Frequency (tFr) has been set at a value higher than 599 Hz.
Resolution:
For invalid configuration, check the configuration loaded previously or load a compatible configuration.
For Max Frequency (tFr) set to high, set the value lower than 599 Hz. Due to safey, variable frequency drives cannot run at 600Hz and above.
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: