{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

How do I set up PID for sleep wakeup on an ATV21 or ATV212 drive?

Issue:
Sleep Wake Up function

Product Line:
ATV212, ATV21

Environment:
All model and serial numbers

Cause:
None

Resolution:
For PID setup see FAQ FA230136.

PID SLEEP WAKEUP can be activated by setting F256 [Time limit low spd]
Setting this function to 0 disables this function.
The range of this function is between 0 and 600 seconds.  0 deactivate this function.

If parameter F256 is activated and if the drive operates continuously at [Low limit frequency] (LL) for a time period equal to the setting of F256, the drive will ramp the motor to a stop. While the motor is stopped, “LStP” will flash on the drive
embedded display terminal.

When the speed reference to the drive exceeds the low speed level LL+F391, the drive will accelerate the motor to the new speed
reference.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: