{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What type of overload comes with the GV2, GV3 and GV7 manual starter and protector?
Issue:
GV Manual Motor Starter and Overloads' class

Product Line:
GV type Tesys manual starters.

Environment:
Tesys manual starters

Cause:
Determination of overload type furnished with the Tesys GV manual motor starters.

Resolution:
The overloads supplied with the GV2, GV3, and GV7 manual starters are Class 10, ambient compensated bimetallic.

Schneider Electric Global