{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Why does Vista crash when I try to start it? I don't even get to the login screen.
Issue:
I have done a Side-By-Side upgrade of a ION Enterprise 6.0 or earlier system to PME 7.2.x or PME 8.0. When I try to start Vista, I get a Windows dialog stating that 'Vista has stopped working.' with options to either 'Check online for a solution and close the program' or 'Close the Program'. I do see the splash screen, but I don't get as far as the login screen before Vista crashes.


Product Line:
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.0

Environment:
Power Monitoring Expert Software Upgrade

Cause:
This will happen if the config\cfg\ud directory includes a file called 'global.log' that was imported from your old system. The global.log file will be present if you have added a global event viewer. The newer version of Vista cannot process the old global.log file, as the old file format from ION Enterprise 6.0 or earlier is not compatible with PME 7.2.x or greater vista. Thus vista crashes.

Resolution:

*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).

Delete global.log from the Install Path\config\cfg\ud directory. Re-add a Global Event Viewer once Vista has started.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.