{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the Altivar drives state when the auto decel ramp adapt feature bRA is engaged?
Issue:
Drives state when the auto decel ramp adapt feature is engaged
Product Line:
Alitvar ATV61, ATV71, ATV312, ATV31, ATV58, ATV12
Environment:
All
Cause:
Needs to know the status of the drive when auto decel ramp adapt is activated.
Resolution:
When the stop order is given, the drive state is "DEC" and if this is needed (brA=Yes) the drive will raise the deceleration time but the state stays to "DEC" until the motor is stopped then the state goes in "rdY".

Schneider Electric Global

Attachment(s)
brA settings.pdf [79.98 KB]