Search FAQs
How do you set the overload setting on the ATS48 soft starters?
Issue:
Programming Overload setting on the ATS48 soft starters
Product Line:
Altivar ATS48
Environment:
All
Cause:
Needs to set the overload settings.
Resolution:
Main menu arrow down to PRO enter
find tHP code enter
Your motor thermal protection options are going to be
Class 30
Class 25
Class 20 (Severe application)
Class 15
Class 10 (Standard application)
Class 10A
Sub Class 2
OFF: No Protection.
You can set your overload current set value in the SET menu
IN= set to the FLA or full load amps of your motor name plate.
Released for:Schneider Electric Global
Attachment(s)
Explore more
Range:
Explore more
Range: