{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Does the Modbus Plus driver suite work with Windows 2008 Server R2?
Issue:
Is there a version of the Modbus Plus driver that will support Windows 2008 Server R2?

Product line:
Modbus Plus

Environment:
MBX driver software

Cause:
Software not working with Windows 2008 Server R2.

Resolution:

Version 7.1 supports Windows Server 2008 R2 and version 8.0 supports Windows 8 and Windows Server 2012.

As of 1/31/2019 Version 9 of the drivers are out and they support Windows 10.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: