Issue:
Using TM2 modules with the M221
Product line:
TM221
Environment:
EcoStruxure Machine Expert Basic (formally SoMachine Basic)
Cause:
Twido obsolete and replacement is the M221
Resolution:
Yes, but the TM2 modules have to be mounted after any TM3 modules if TM3 modules are used.
Using TM2 modules with the M221
Product line:
TM221
Environment:
EcoStruxure Machine Expert Basic (formally SoMachine Basic)
Cause:
Twido obsolete and replacement is the M221
Resolution:
Yes, but the TM2 modules have to be mounted after any TM3 modules if TM3 modules are used.
Released for:Schneider Electric Global
Issue:
Using TM2 modules with the M221
Product line:
TM221
Environment:
EcoStruxure Machine Expert Basic (formally SoMachine Basic)
Cause:
Twido obsolete and replacement is the M221
Resolution:
Yes, but the TM2 modules have to be mounted after any TM3 modules if TM3 modules are used.
Using TM2 modules with the M221
Product line:
TM221
Environment:
EcoStruxure Machine Expert Basic (formally SoMachine Basic)
Cause:
Twido obsolete and replacement is the M221
Resolution:
Yes, but the TM2 modules have to be mounted after any TM3 modules if TM3 modules are used.
Released for:Schneider Electric Global