Search FAQs
Can the finger-style vertical cable managers for 600 mm cabinets be installed on the same 0U Accessory Channel as a PDU?
Issue:
Customers may want to mount a PDU on the accessory channel behind the vertical cable manager.
Product Line:
NetShelter SX
Environment:
AR7721, AR7722, AR7723
Cause:
The installation manual of the Cable Managers for 600 mm cabinets shows the cable manager being installed over both PDU mounting areas of the 0U accessory channel.
Resolution:
The vertical cable manager can be installed in the rear-most facing position so that a PDU can be mounted behind it.
Customers may want to mount a PDU on the accessory channel behind the vertical cable manager.
Product Line:
NetShelter SX
Environment:
AR7721, AR7722, AR7723
Cause:
The installation manual of the Cable Managers for 600 mm cabinets shows the cable manager being installed over both PDU mounting areas of the 0U accessory channel.
Resolution:
The vertical cable manager can be installed in the rear-most facing position so that a PDU can be mounted behind it.
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: