Search FAQs
Is it possible to change application type of my Sepam?
Issue
Is it possible to change application type of my Sepam
Product Line
Sepam series 20
Sepam series 40
Sepam series 80
Environment
Application Type
Cause
Would like to change the application type of Sepam relay
Resolution
The answer is a little bit different according to the Sepam series:
Is it possible to change application type of my Sepam
Product Line
Sepam series 20
Sepam series 40
Sepam series 80
Environment
Application Type
Cause
Would like to change the application type of Sepam relay
Resolution
The answer is a little bit different according to the Sepam series:
- Sepam series 20 and 40: Modification of Sepam application type requires replacement of your complete Sepam. You need to order a new Sepam with the correct application type needed.
- Sepam series 60 and 80: As application type is in the cartridge, modification of Sepam application type requires only replacement of the cartridge. You need to order a new cartridge with the application type needed. Note: be careful, since you may need to purchase additional CCA63x CT adapters, depending on which Application Types are involved.
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: