{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Video: How can you program the ATV21 or ATV212 drive so that you can run the drive without the motor?

Article available in these languages: Finnish

Issue:
Configuring ATV212 Drive to Run Without Motor Connected

Product Line:
Altivar ATV21 ATV212 S-Flex enclosed

Environment:
All

Cause:
Need to test the drive to see if there is a problem with it or a need to run the drive open circuit without the motor connected to it.

Resolution:
Programming
Find F- - - Enter
Scroll to Output Phase Loss F605= 0 (deactivate)
Set supply voltage correction F307 to 2 (supply voltage uncorrected).
Now you can disconnect your motor leads, and run the drive open circuit to test.


Be sure to return the parameters to their original value once testing has been completed.

Schneider Electric Global

Attachment(s)
ATV212_Programming_manual_EN_S1A53838_01.pdf [3.49 MB]