{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
When did the ATV18 drive become obsolete?
Issue:
Is the ATV18 become obsolete?

Product line:
ATV18, Altivar 18

Environment:
All models, all serial numbers

Cause:
Determine age of unit, product obsolescence

Resolution:
ATV18 became obsolete in 1995.
The current replacement is the ATV12, ATV312 or ATV320 depending on the application (Current, HP and Voltage of the motor).
There are some differences in dimensions, wiring and programming that should be reviewed by the customer.

Schneider Electric Global

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: