{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

What's the different between Modbus TCP server and Modbus TCP slave device for M258 Ethernet?

Modbus TCP serverModbus TCP slave device
Only configure IP addressNeed to configure parameters and I/O mapping
For Modbus TCP client, all %MW address of server can be R/W.For I/O scanner, only %IW area (2~40 words) can be R/W, %QW area (2~40 words) are read only, and actual %MW address of slave device cannot be visited.
No need to configure “Unit ID”Unit ID (1~247) should be same the unit ID setting in Modbus TCP I/O scanner.
No visualized list for communicated address.Have a clear and visualized interface to monitor all communicated variables.
The connection to one client may be closed when more than 8 connections are needed.The connection to the Master client is never forcefully closed, when IPMaster Address is configured.

Please see attached ModbusTCP Slave Device explanation document.

Schneider Electric Global

Attachment(s)

Modbus TCP Slave Device.pdfModbus TCP Slave Device.pdf [89.91 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: