{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

Are the 8903L, 8903LX, and 8903S Square D lighting contactors rated for LED lighting applications?

Issue:
Documentation for LED lighting loads or ratings for 8903L or 8903LX lighting contactors?

Product Line:
Class 8903 Type L/LX Lighting Contactors

Environment:
NEMA Lighting Contactors

Cause:
Application information

Resolution:

As of 2017 Schneider Electric has tested the Class 8903 Type L/LX and Type S NEMA lighting contactors per NEMA-410-2015 and UL508: Table 46.1 and Section 61C.
(Test procedures for LED Loads).

This test specifies procedures up to 16A loads at 120VAC. Our testing was performed at 20 amps 120VAC and passed all of the requirements

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: