Issue
For the HMIGTO series of HMI, is there an option with conformal coating?
Are they different than the HMIGTO with steel bezels?
Product Line
Harmony HMIGTO
Environment
Physical HMI for harsh environments
Resolution
Yes, there are conformal coating options for the HMIGTO HMIs.
The part numbers are the same as the regular HMIGTOs, except they end with a "FCW"
HMIGTO1300FCW (3.5")
HMIGTO1310FCW (3.5")
HMIGTO2300FCW (5.7")
HMIGTO2310FCW (5.7")
HMIGTO3510FCW (7.0")
HMIGTO4310FCW (7.5")
HMIGTO5310FCW (10.4")
HMIGTO6310FCW (12.1")
The Conformal Coating units are different than the units with Stainless Steel Bezels with the '5' suffix in the last digit of the part numbers.
Note that there are only 3 models available for the Stainless Steel Bezel HMIGTOs - screen sizes 5.7', 10.4", and 12.1":
HMIGTO2315 (5.7")
HMIGTO5315 (10.4")
HMIGTO6315 (12.1")
The Stainless Steel Bezel units ending with '5' in the part number cannot be ordered with conformal coatings.
For the HMIGTO series of HMI, is there an option with conformal coating?
Are they different than the HMIGTO with steel bezels?
Product Line
Harmony HMIGTO
Environment
Physical HMI for harsh environments
Resolution
Yes, there are conformal coating options for the HMIGTO HMIs.
The part numbers are the same as the regular HMIGTOs, except they end with a "FCW"
HMIGTO1300FCW (3.5")
HMIGTO1310FCW (3.5")
HMIGTO2300FCW (5.7")
HMIGTO2310FCW (5.7")
HMIGTO3510FCW (7.0")
HMIGTO4310FCW (7.5")
HMIGTO5310FCW (10.4")
HMIGTO6310FCW (12.1")
The Conformal Coating units are different than the units with Stainless Steel Bezels with the '5' suffix in the last digit of the part numbers.
Note that there are only 3 models available for the Stainless Steel Bezel HMIGTOs - screen sizes 5.7', 10.4", and 12.1":
HMIGTO2315 (5.7")
HMIGTO5315 (10.4")
HMIGTO6315 (12.1")
The Stainless Steel Bezel units ending with '5' in the part number cannot be ordered with conformal coatings.
Released for:Schneider Electric Global
Issue
For the HMIGTO series of HMI, is there an option with conformal coating?
Are they different than the HMIGTO with steel bezels?
Product Line
Harmony HMIGTO
Environment
Physical HMI for harsh environments
Resolution
Yes, there are conformal coating options for the HMIGTO HMIs.
The part numbers are the same as the regular HMIGTOs, except they end with a "FCW"
HMIGTO1300FCW (3.5")
HMIGTO1310FCW (3.5")
HMIGTO2300FCW (5.7")
HMIGTO2310FCW (5.7")
HMIGTO3510FCW (7.0")
HMIGTO4310FCW (7.5")
HMIGTO5310FCW (10.4")
HMIGTO6310FCW (12.1")
The Conformal Coating units are different than the units with Stainless Steel Bezels with the '5' suffix in the last digit of the part numbers.
Note that there are only 3 models available for the Stainless Steel Bezel HMIGTOs - screen sizes 5.7', 10.4", and 12.1":
HMIGTO2315 (5.7")
HMIGTO5315 (10.4")
HMIGTO6315 (12.1")
The Stainless Steel Bezel units ending with '5' in the part number cannot be ordered with conformal coatings.
For the HMIGTO series of HMI, is there an option with conformal coating?
Are they different than the HMIGTO with steel bezels?
Product Line
Harmony HMIGTO
Environment
Physical HMI for harsh environments
Resolution
Yes, there are conformal coating options for the HMIGTO HMIs.
The part numbers are the same as the regular HMIGTOs, except they end with a "FCW"
HMIGTO1300FCW (3.5")
HMIGTO1310FCW (3.5")
HMIGTO2300FCW (5.7")
HMIGTO2310FCW (5.7")
HMIGTO3510FCW (7.0")
HMIGTO4310FCW (7.5")
HMIGTO5310FCW (10.4")
HMIGTO6310FCW (12.1")
The Conformal Coating units are different than the units with Stainless Steel Bezels with the '5' suffix in the last digit of the part numbers.
Note that there are only 3 models available for the Stainless Steel Bezel HMIGTOs - screen sizes 5.7', 10.4", and 12.1":
HMIGTO2315 (5.7")
HMIGTO5315 (10.4")
HMIGTO6315 (12.1")
The Stainless Steel Bezel units ending with '5' in the part number cannot be ordered with conformal coatings.
Released for:Schneider Electric Global