Issue
Mcafee Virus Scanner detects 'Credits.exe' from 'ProWORX 32' as an infected file.
Product Line
ProWORX 32
Environment
Windows 7,Windows 8, Windows 10
Resolution
McAfee Anti-viirus software detects 'Credit.exe' as an infected file.
The 'Credits.exe' file is only used to present a 'Thank for using ProWORX 32' pop-up message window. The file is
not used in any part of the ProWORX 32 software. It can be deleted. The file should be deleted using the delete
function in the anti-virus software.
Attempts to delete the file from a folder may fail.
Mcafee Virus Scanner detects 'Credits.exe' from 'ProWORX 32' as an infected file.
Product Line
ProWORX 32
Environment
Windows 7,Windows 8, Windows 10
Resolution
McAfee Anti-viirus software detects 'Credit.exe' as an infected file.
The 'Credits.exe' file is only used to present a 'Thank for using ProWORX 32' pop-up message window. The file is
not used in any part of the ProWORX 32 software. It can be deleted. The file should be deleted using the delete
function in the anti-virus software.
Attempts to delete the file from a folder may fail.
Released for:Schneider Electric Global
Issue
Mcafee Virus Scanner detects 'Credits.exe' from 'ProWORX 32' as an infected file.
Product Line
ProWORX 32
Environment
Windows 7,Windows 8, Windows 10
Resolution
McAfee Anti-viirus software detects 'Credit.exe' as an infected file.
The 'Credits.exe' file is only used to present a 'Thank for using ProWORX 32' pop-up message window. The file is
not used in any part of the ProWORX 32 software. It can be deleted. The file should be deleted using the delete
function in the anti-virus software.
Attempts to delete the file from a folder may fail.
Mcafee Virus Scanner detects 'Credits.exe' from 'ProWORX 32' as an infected file.
Product Line
ProWORX 32
Environment
Windows 7,Windows 8, Windows 10
Resolution
McAfee Anti-viirus software detects 'Credit.exe' as an infected file.
The 'Credits.exe' file is only used to present a 'Thank for using ProWORX 32' pop-up message window. The file is
not used in any part of the ProWORX 32 software. It can be deleted. The file should be deleted using the delete
function in the anti-virus software.
Attempts to delete the file from a folder may fail.
Released for:Schneider Electric Global