undefined [object Object]
{}

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the maximum distance for the TM3 (TM3XTRA1 / TM3XREC1) transmitter and receiver modules?
Issue
What is the maximum cable length between the Modicon TM3 transmitter (TM3XTRA1) and receiver (TM3XREC1) modules?

Product Line
Modicon TM3 Expansion I/O modules for M221, M241, M251, M262 PLCs

Environment
Physical PLC

Resolution
5m (16.4ft) is the maximum length between the TM3 transmitter (TM3XTRA1) and receiver (TM3XREC1) modules.
The part number of the recommended cable is VDIP184546050 (5.0 m).

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: