{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

What replacement enclosures are available for the 8903 Type L and LX lighting contactors?

Issue:
Enclosures for Class 8903 Type L and LX lighting contactor.

Product Line:
8903 NEMA Lighting Contactors

Environment:
NEMA Contactors and Starters

Resolution:
Options include the following,
NEMA 1 - Surface Mount Enclosure:  9991LXG1
NEMA 3R - Enclosure:  9991SDH1
NEMA 4  - Standard Enclosure:  9991SDW1
NEMA 4  - With 2 Cover Mtd. Closing Plates:  9991SDW11
NEMA 4X - Glass Polyester Enclosure:  9991SDW20
NEMA 12 - Enclosure:  9991SDA11

NEMA 1 Flush Mount Parts:
Cover:  9991SDF13
Mounting Strap:  9991SDF2
Pull Box:   9991SDF1

Oversized enclosures (where cover mounted controls are needed):
NEMA 1:  9991SDG3
NEMA 4:  9991SDW3
NEMA 12:  9991SDA3

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: