Issue
Need to program the VAMP relay with the IEC61850 communication.
Product Line
VAMP 5x, 2xx, 3xx
Environment
VAMP set and SCD Editor
Resolution
Attached are the manuals for programming the VAMP for IEC61850
Latest information is available in m.vamp.fi
Need to program the VAMP relay with the IEC61850 communication.
Product Line
VAMP 5x, 2xx, 3xx
Environment
VAMP set and SCD Editor
Resolution
Attached are the manuals for programming the VAMP for IEC61850
Latest information is available in m.vamp.fi
Released for:Schneider Electric Global