{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What are the Publish and Receive Gooses Capacity for Sepam and CET 850 in IEC61850 Protocol?
Issue
Customer would like to know the capacity for GOOSE messaging.

Product Line
IEC 61850
Sepam 80 Series

Environment
communications

Resolution
For GOOSE publishing there isn't a maximum limit. Only the limit to 100% has to be respected.

For GOOSE receive messages there are a maximum of 40 GOOSE subscriptions for each IED/ ICD file.
For each Sepam there are 31 GOOSE receive messages when using the SFT 2841 to program.

Schneider Electric Global