{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

Failed to Connect to the SEPAM front face using the USB cable.

Issue
When trying to connect to the SEPAM using SFT2841 with the mini USB to USB (CCA784) it fails.

Product Line
SFT2841

Environment
Windows computer management

Cause
The driver for windows is not get install or cannot find it.

Resolution
Attached are the work around for the XP and Windows 7 operating systems.  If one as Windows 7 or above follow the Windows 7 pdf.

Schneider Electric Global

Attachment(s)

Computer connection to sepam with USB front panel - WinXP.pdfComputer connection to sepam with USB front panel - WinXP.pdf [640.67 KB]
Computer connection to sepam with USB front panel-Win7.pdfComputer connection to sepam with USB front panel-Win7.pdf [817.22 KB]
Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: