Search FAQs
Can we skip to the latest Vijeo Designer Service Pack?
Issue:
Can we skip to the latest Vijeo Designer Service Pack?
Product Line:
Vijeo Designer (all versions)
Resoluton:
Since Vijeo Designer Service Packs are cumulative, Vijeo Designer VX.y SPz would contain the same fixes as Vijeo Designer VX.y SP(z-1). Therefore yes, it is possible to skip to the latest Vijeo Designer Service Pack without installing the previous versions.
Ex. Vijeo Designer V6.2 SP3 contains Vijeo Designer V6.2 SP2 and Vijeo Designer V6.2 SP1.
Keep in mind that it is possible that some hotfixes are not in the service pack that is immediately next (ie version SPn). This is indicated by a build number of 5000 or greater for the hotfix. The hotfix content in this case will be available in the next service pack (ie. SPn + 1)
Can we skip to the latest Vijeo Designer Service Pack?
Product Line:
Vijeo Designer (all versions)
Resoluton:
Since Vijeo Designer Service Packs are cumulative, Vijeo Designer VX.y SPz would contain the same fixes as Vijeo Designer VX.y SP(z-1). Therefore yes, it is possible to skip to the latest Vijeo Designer Service Pack without installing the previous versions.
Ex. Vijeo Designer V6.2 SP3 contains Vijeo Designer V6.2 SP2 and Vijeo Designer V6.2 SP1.
Keep in mind that it is possible that some hotfixes are not in the service pack that is immediately next (ie version SPn). This is indicated by a build number of 5000 or greater for the hotfix. The hotfix content in this case will be available in the next service pack (ie. SPn + 1)
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: