{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
ADVC Controller Test and Training Set does not show the correct series
Issue
When the test and training set (TTS) is connected to the ADVC Controller it is showing a U-Series Recloser instead of a N-Series Recloser.

Product Line
ADVC II, Recloser, U-Series, N-Series, and W-Series

Environment
Testing the Recloser settings.

Cause
The old calibration files took the form of the first Recloser series that the TTS connects to.  The series cannot be changed after that.

Resolution
In order to have the TTS have the ability to switch between series the calibration file needs to be N24-150s (24kV 150kV BIL 1A CT's).
Attached is the calibration file, instructions on how to check the calibration file and how to load the file, and application notes about the calibration file.

Note:  The firmware of the ADVC Controller firmware must be A45-11.01 or above.

Schneider Electric Global

Attachment(s)
SN392796.zip [511 Bytes]
Schneider Reclosers ADVC Writing .cal file to TTS 1.0.pdf [300.92 KB]
Application Notes A45 multiple switch series TTS R03.pdf [24.63 KB]
Explore more
Range:
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: