{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What type of Communication Modules are available for the SEPAM Relays?
Product Line
SEPAM Communications

Environment
Networking and communications

Resolution
The protocols that are available are:  DNP3, Modbus RTU, IEC 60870-5-103, Modbus TCP/IP, and IEC61850.  Not all modules have the same type of protocols or type of communications.  Attached is the communication accessory selection guide to help pick the correct module.

Schneider Electric Global

Attachment(s)
Communication Selection Guide.pdf [109.74 KB]