Search FAQs
What is the communications cable between the Magelis XBTN200 / XBTN400 and Modicon M221 controller?
Issue:
What is the communication cable needed between an M221 and XBTN.
Product Line:
M221
XBTN200
XBTN400
Resolution:
Tthe communications cable between the XBTN400 and M221 is XBTZ9980
This is a Modbus RS485 communication cable.
What is the communication cable needed between an M221 and XBTN.
Product Line:
M221
XBTN200
XBTN400
Resolution:
Tthe communications cable between the XBTN400 and M221 is XBTZ9980
This is a Modbus RS485 communication cable.
Released for:Schneider Electric Global
Attachment(s)
Explore more
Range:
Explore more
Range: