{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can I use the service port on the M580 HSBY processor for SCADA traffic while servicing ERIO ?
Not recommended. Please consider using an NOC module. The service port does not support Rapid Spanning Tree Protocol and as a result the connection of each of these ports to a SCADA can result in an excessive amount of broadcast or ARP traffic.

We recommend using the NOC option module for SCADA in HSBY applications.

Schneider Electric Global