{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

Video: How do you set up a command switch via logic input on the ATV630 and ATV930 drives?

Article available in these languages: Finnish, Dutch

Issue:
How do you set up a command switch via logic input on the ATV630 and ATV930 drives?

Product Line:
Altivar Process ATV630 and ATV930 drives

Environment:
All

Cause:
Need to use a logic input to switch between two command functions like HMI start stop and terminal start stop.

Resolution:
Programming
Press the Home button.
Scroll down to menu 5 complete settings enter.
Scroll down to menu 5.5 command and references enter
Scroll down and choose command switching and assign it to DI3 enter
Scroll down and choose CMD channel 1 for your first command and CMD 2 for your second command.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: