{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

Can the Magelis HMIG5U/HMIG5U2/HMIG5U22 print to a Windows Printer?

Issue:
Can the Magelis HMIG5U/HMIG5U2/HMIG5U22 print to a Windows Printer?

Product Line:
HMIGTU

Resolution:
Yes, you use the Windows Default as the printer in Vijeo Designer for the HMIG5U.

But the drivers may not be compatible with Windows 7 embedded.  Some instances the Windows 7 driver is not the same as the embedded drivers.  Or there might be a "special" way to install the drivers.

Please check with the manufacturer of the Printer to confirm the driver will support in a Windows 7 Embedded operating system before purchasing a printer to use in Runtime.

Schneider Electric Global