Search FAQs
What is the standard overload range for form H30 on an 8536 type S starter?
Issue:
SSOLR code for 8536 type S Starter
Product Line:
NEMA Type S starters
Environment:
Type S Full Voltage Contactors and Starters
Resolutions:
The standard overload range will depend on the starter size. Note the range can be changed. Check the Digest for details on modifying the form.
SSOLR code for 8536 type S Starter
Product Line:
NEMA Type S starters
Environment:
Type S Full Voltage Contactors and Starters
Resolutions:
The standard overload range will depend on the starter size. Note the range can be changed. Check the Digest for details on modifying the form.
Size | 00 | 0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 (SSOLR comes standard) |
Amp Range | 3-9 | 6-18 | 9-27 | 15-45 | 30-90 | 45-135 | 90-270 | 180-540 | 270-810 |
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: