{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

Do the Altivar Process Drives come with a DC choke or Line Reactor?

Article available in these languages: Japanese

Issue:
DC choke or Line Reactor included on Process Drives?

Product Line:
Altivar Process Drives (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)

Environment:
All serial numbers for Altivar Process Drives

Cause:
N/A

Resolution:
All Altivar Process Drives come standard with DC chokes.
There is no need for a line reactor.

ATV...M3 (208/240 Vac)
Double DC choke up to Frame Size 3
Single DC choke for Frame Size 4 and upwards

ATV....N4 (400/480 Vac)
Double DC choke up to Frame Size 4
Single DC choke for Frame Size 5 and upwards
NOTE:
The Size 7 ATV630 product and the Size 7A and 7B ATV930 products come standard with the DC Choke, but can be ordered without the DC Choke by adding a suffix MN to the part number.
When not using the DC Choke a 5% input line reactor or line choke MUST be used.
Example:  ATV630C22N4 includes a DC Choke   ATV630C22N4MN does not include a DC Choke.
Drive Systems and Floor Standing
All Drive Systems and Floor Standing Products have as standard embedded line chokes and optional motor chokes.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: