{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Could you advice whether we could ship/deliver Blokset/Okken panel in horizontal position?
No. It is not advisable to transport the BlokSeT/Okken Panel in Horizontal position.

The panels are intended to be used in vertical position. During the designing of the panel, care has been taken to ensure to withstand the forces which is generated because of vibration in vertical position only.
During transportation in horizontal position, the Devices, busbars and sheet metal parts may get damage because of the vibrations generated during the transportation. This will affect the performance of the switchboard.

So, we do not advise transporting in Horizontal position. It should be always in Vertical position only.

Schneider Electric Global