{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

Are the ATV320 drives backward compatibility with ATV32 on Profibus?

Article available in these languages: Spanish

Issue:
ATV320 and ATV32 Backward compatibility on Profibus

Product Line:
ATV320

Environment:
All

Cause:
Profibus compatibility

Resolution:
Concerning the Profibus functions and programming, yes this will be the same between the ATV32 and ATV320 B or C.
The point will be in case of ATV32 replacement by ATV320 without changing the GSD file PLC programming: the PLC will not see the 320 drive.
ATV32 has it's own GSD file and ATV320 also has it's own GSD file. When you will replace ATV32 by ATV320, you need to add this ATV320 GSD file in the PLC to have ATV320 operating.

After this update of PLC with the ATV320 GSD file, the configuration and functions available on ATV320 will be the same as ATV32.

Schneider Electric Global

Explore more
Range:
Altivar Machine ATV320
Explore more
Range:
Altivar Machine ATV320
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.