{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How do I troubleshoot an Altivar Process Drive that would not connect or communicate to a DeviceNet device or network?

Article available in these languages: Spanish

Issue:
Altivar Process Drive that will not connect or communicate with a DeviceNet device or network.

Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)

Environment:
All serial numbers for Altivar Process Drive

Cause:
N/A

Resolution:

Note: This FAQ goes over some basic checks and troubleshooting tips. For extended troubleshooting please refer to your drives DeviceNet manual.

Drive Will Not Connect
  • Communication Module
    • DeviceNet is not integrated on the Altivar Process drives. Must use module VW3A3609.
    • The VW3A3609 Fieldbus module, with a minimum V1.6IE01 firmware version, is compliant with the Altivar process product range.
    • Only one communication module can be used at a time
  • Installation
  • Network
    • Check for any duplicate addresses on the network.
    • Check to make sure you have proper configured assemblies
  • Programming
    • Check Basic Settings on the drive. Make sure the following is set:
      • IP Address
      • Baud Rate
      • Data rate used
      • Make sure drive is power cycled after any Communication settings are changed.
    • Check for properly configures assemblies
  • Troubleshooting
    • Check LEDs on the drive
      • See Fieldbus Status LEDs, LED MS Network Status and LED MS Module Status  attachments
      • Drive Connects But Will Not Run
  • Network
  • Programming on the Drive
    • Confirm drive is setup for Network Control
      • Check Command and Reference Menu
        • [Complete settings] [Command and Reference]
  • ​​Troubleshooting
    • Check Communication Map
      • [Display] [Communication map]
        • ​​Check Command Channel
        • Command Register
        • Ref Freq Channel
        • Ref Freq
Reference attached manuals for further troubleshooting

Schneider Electric Global

Attachment(s)
ATV600_DeviceNet_Manual_EN_EAV64330_01.pdf [3.47 MB]
ATV600_Programming_Manual_EN_EAV64318_04.pdf [10.52 MB]
ATV900_DeviceNet_Manual_EN_NHA80942_01.pdf [5.2 MB]
ATV900_Programming_Manual_EN_NHA80757_02.pdf [11.22 MB]
LED NS Network Status.png [150.18 KB]
Fieldbus Status LEDs.png [91.26 KB]
LED MS Module Status.png [217.56 KB]