{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
My Micro DC came with clamp-on ferrites. Where do they go, and are there installation instructions?
Issue:
The Micro DC SX ships with clamp-on ferrites. I don't know where they go or how to install them.

Product Line:
Micro DC SX,

Environment:
24U and 48U SX EMEA units only

Cause:
The Micro Data Center SX International units ship with one snap-on ferrite per piece of installed equipment.

Resolution:
Ferrite is installed onto the network communications cable to reduce high frequency RF interference, and is required for 50 Hz operation.
See attachment for installation instructions.

Schneider Electric Global

Attachment(s)
Snap on ferrite clamps.docx [63.19 KB]